AXIS#.HOME.V

Description

AXIS#.HOME.V is the velocity used while homing. When searching for an index this speed is reduced by AXIS#.HOME.CREEPFACTOR.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS.

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

60 RPM

Depends on units. See Velocity Units for details.

Data Type

Float
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
AXIS1.HOME.V

5008h

10h

Unsigned32

Velocity

-

Read/Write

No

AXIS2.HOME.V

5108h

10h

Unsigned32

Velocity

-

Read/Write

No

AXIS1.HOME.V

6099h

01h

Unsigned32

Velocity

-

Read/Write

No

AXIS2.HOME.V

6899h

01h

Unsigned32

Velocity

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.V

6112

17E0

Signed32

Read/Write

Velocity

AXIS2.HOME.V

71648

117E

Signed32

Read/Write

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.V

6112

Float

Read/Write

Velocity

Related Topics

Homing